DSO203 GCC APP - Community Edition (2.51+SmTech1.8+Fixes)

Greetings Ponti



Welcome here.



It is very easy to upgrade your device to run Wildcat version of the firmware.


  1. Download the archive from this thread.


  2. Extract the .HEX files somewhere you can find them


  3. Connect the DSO to your PC via USB.


  4. Press and hold the first button of DSO and switch on the DSO. You will see a different screen on the DSO. A new drive will appear on your Windows machine.


  5. Now, you can copy any one of the HEX files to the DSO drive on your machine(remember which HEX you copied). The PC will beep to indicate USB disconnect and again USB connect.


  6. Turn off the DSO and you may disconnect USB now.


  7. Press button on DSO as per hex file number you loaded. If you loaded app2.hex, you press button 2 and power on the DSO and so on. For App1.hex, you should not press button 1 as it will bring you back to step 4.


  8. Voila, new firmware is running.



    Good luck