DSO203 GCC APP - Community Edition (2.51+SmTech1.8+Fixes)

What happens when you boot up? Do you see the startup screen with hardware,

FPGA, system version, program version and so on? Or does it just go directly to a blank screen?



If it shows the startup screen, there will be a message showing whether the

program loaded a config file: if it found a file it will read “Reload parameter from disk”.

If no file is found you will see “Parameters not found” or something like that.

If a config file is loaded and it freezes up after that, you should delete any

XXXXX.WPT on the flash drive; you will need to boot up to a running program

and connect to a computer via USB to do this. It’s possible a corrupt config

file may be causing this. Earlier versions used a WPT extension for their

config files, but I think the later (with 8Mb devices) versions use a different extension.



If it goes directly to a blank screen something likely got corrupted.



Can you load any other programs into slot 1 (or any other) and have them work?

I take it you get the .rdy file after copying the hex file when you instal the program

with the bootloader? If other programs load/run OK and there is no WPT config file

on the device maybe the HEX file got corrupted somehow?