DSO203 GCC APP - Community Edition (2.51+SmTech1.8+Fixes)


Yes, pawn is ok for me too !

I have two files : CALIB.DAT and CALIBRAT.INI (which I saved elsewhere)

I think they are for APP110 and Pawn when I have it (APP110 is now installed on slot 3 and it uses slot 3/4, so I don’t have pawn working anymore : not surprising.)


My problem is actually with SYS1.6, alterbios seems to not install anything. (How to be sure it is installed ?)

I have tried Sys1.52 and the community app wasn’t saving anything…

I don’t remember if I tried at this moment AlterBios, but I think I did.



Pehaps the good combination is the older SYS, alterbios0.4 and the community app : to be tried…



My other concern is gabonator, really good and working with sys 1.6 (I can save parameters, but others files corrupts the memory, and I lose calibration, and because It is not stored on the flash memory, I can’t restore it.

<LINK_TEXT text=“http://www.seeedstudio.com/forum/viewto … 441#p18441”>DS203 quad user interface design - #98 by fflan - DSO Quad - Seeed Studio Forum</LINK_TEXT>



An ideal configuration would be (for me) : Gabonator and the community APP fully working, with or without Pawn

OR

Gabonator and Pawn

OR

Community APP and Pawn

The main fault on the origina APP is tension and zero V accuracy, ridiculous…and well adressed by the two others;…



Thanks for your help