DSO203 GCC APP - Community Edition (2.51+SmTech1.8+Fixes)

Is it just me or does the display not refresh properly when using 200uS/div. or 500uS/div. horizontal sweep? The very left-most column of pixels in the waveform display jumps all over the place with the input signal, but the rest of the waveform does not update as well. If I set “TrOFF” and give up triggering it seems to update fine. Is this a problem with the way triggering is performed? No combination of trigger settings alleviate the issue other than disabling it in those timescales.



Has anyone else experienced this issue? Is there a work-around?