Hi,
I have downloaded the app (GCC) version 1.24 and successfully installed in my device. But the the long press to (play/pause) button is not showing any FFT. the long press to square button is showing corrupted text in calibration window :roll:.
I have already successfully updated the the latest FPGA and SYS files and the official app is running perfectly. Also the gabonator app is running properly. The reason for looking for non-official UI is that the official UI can not show the low frequency (a few Hz) signal smoothly. It takes a lot of time to fill its buffer and than all of a sudden shows a frame, after 10s of seconds. This problem is there even the gabonator UI and even do not allow me to set time base to 1s.
Thanks in advance for any suggestion.