Good job folks!
I have two of these and they’re really great. First came with Sys version 1.51 and App version 2.52. The second was bought this year and came with Sys version 1.51 and “App (plus A1) Version 1.00”, of which more later. I have flashed your V1.24 APP_G251.hex, which is much better than the 2.52, with some great features and bug fixes. Note that I’ve left it on SYS 1.51 for now and it seems to work except spectrum analyser. I’d like to try Wildcat’s version for comparison, which is why I left 1.51 sys, but I can’t seem to get it to work: I upload the three .HEX files, appx.hex, then renamed to app_0001.hex, then renamed to APP_0001.HEX, then loaded on with power cycle in-between files, but all I get is the boot screen with the buzzer stuck on. What am I doing wrong?
Thanks.