DSO Quad bandwidth

Unfortunately simulators don’t tell the truth at these gain and frequency levels. The biggest problem would be getting stability and I suspect that C9 C11 and C73 were added later to acheive stability. Removing them is probably not an option. PCB layout is everything and having gain switching really makes the layout difficult because the + and - input nodes of the op amps need to be as short as possible. It should be possible to get 15nS rise time with the 27MHz circuit above but it will be difficult. Might be an idea to build up a simple fixed gain circuit first.