If the gain resistors are reduced and front end optimized as is then theoretically one can get up to 10MHz overall flat response @ G=10 according to the OPA2354 datasheet which makes sense. The corrected circuit is shown below. The C9 and C11 10pF caps should be lifted as well as C7A. Feedback resistors should be reduced as much as possible while maintaining the necessary gain.
According to the plots these changes shift the 3dB point for both signals up to 12MHz which in reality is overly optimistic. I’d say 10MHz BW is more realistic but still hard to achieve as it is highly dependent on the PWB layout.