Ok, I decided to model the front end of the analog channels, which was done on Multisim.
Here are the results:
The 3dB point for signal 1 about 700kHz and for signal 2 is about 200kHz.Looking at these large resistors in the front end the results do not surprise me actually – the RC constants are far stretch from minimized. The resistances in the op-amps feedback loops are also way too large to expect overall wide BW. Realistically the front end should be have been buffered and then scaled and sampled.
Keeping in mind that this simulation is assuming perfect conditions (no stray capacitance at the very least) I’d say that the front end needs some work, but this is just my 2c.