Dear BenF:
The one thing I TRULY NEED to make the DSO201 useful to me is an ‘external trigger’ (with some internal hardware access to use RX). That way at least I can get ‘some’ of the utility of dual-trace to relate an event to the scope data. However, the signal I am sampling looks MUCH more legible using your ‘fast’ ‘peak’ display mode. I have attempted to re-create that ability from the available 3.13 code base, but my result still doesn’t look NEAR as good. Is there ANY chance you could pass along at least Process_Wave() to me at [email protected] that I may have at least that improvement, or at least describe the ‘peak’ algorithm?
BTW, the other trick I am hoping I can get to work is the ‘roll’ mode so that all new samples come ‘in at the right’ and slew toward the left, ala chart paper. For certain slow event-watching this is quite a bit easier to digest than ‘scan’ mode.
Earl Goodrich II