DSO firmware version 3.64

Hi BenF and all users of this forum, excuse my english, i’m not native english speaker

I am new to this forum and to the DSO nano v2.
I installed BenF firmware 3.64
If you ever plan to make an upgrade, I want to point to a feature that is missing, in the frequency generator menu maybe you can add a “burst” function, that can be preset (5, 10, 50, 100 pulses) or can be user defined
you can set frequency
you can set
if you can set a number of pulses to be generated, then the a automotive tool used to verify injector balance become useless, all you need is to make a driver for the injector so it will use the battery power and use the nano to command that driver, the driver can be made with one FET, or any switch transistor able to handle the load.
Also i noticed that the generator is always on, is that consuming resurses?

Anyway thank you very much for your effort into making this firmware.