Hello BenF,
First of All Thanks for your endeavour and the source code of your firmware version 3.11!
About the version 3.20, I tried under Linux (Mint 9 ~ Ubuntu 10.04) to flash it (I did it twice after downgrading to version 3.12), but something is going wrong in my case because I don’t see any trace on the screen (only something which seems to be a small trace in the bottom-right) and the firmware seems to be frozen.
To be fair, I use the dfu-util enhanced by tormod and perhaps it is related to this tool:
[code]dfu-util -V
dfu-util - (C) 2005-2008 by Weston Schmidt, Harald Welte and OpenMoko Inc.
(C) 2010 Tormod Volden (experimental DfuSe support)
This program is Free Software and has ABSOLUTELY NO WARRANTY
dfu-util does currently only support DFU version 1.0
dfu-util version 0.2+
[/code]
here is the command used to flash this firmware:
dfu-util --dfuse default -d 0x0483:0xdf11 -i 0 -D DSO_BenF_LIB_v3.02.dfu
dfu-util --dfuse default -d 0x0483:0xdf11 -i 0 -D DSO_BenF_APP_v3.20.dfu
and in attachment you have the ouputs of this command.
Also too, in attachement there is a picture of the screen (don’t bother with the blue pixel in mid-upper-left, it is a dead pixel on my new DSO Nano v2!) showing its drawing state.
Thank you for reading and Thank you for the last improvment.
DFuse_DSO_BenF_APP-LIB_v3.02-20.dfu.v4.log.tar.bz2 (1.51 KB)