Hi there,
SO , In Zephyr Kconfig, dependencies override your direct config choice.
So even if you manually write CONFIG_DISK_DRIVER_FLASH=y, it gets turned off (n) if its dependency like DT_HAS_ZEPHYR_FLASH_DISK_ENABLED is n.
This is why he sees the warning — not an error, but a heads-up that the config request was ignored.
The unmet dependency is:
DT_HAS_ZEPHYR_FLASH_DISK_ENABLED (=n)
This means that the device tree does not define a “flash-disk” node (usually under /flash, or some partition label).
What’s Missing / Likely Cause:
- The user did not enable or define a proper flash partition (storage node) in their Device Tree overlay (DTS).
- They may also have missed enabling:
CONFIG_FLASH=y
CONFIG_FLASH_MAP=y
CONFIG_FLASH_PAGE_LAYOUT=y
- Without the correct partition label (like
"storage") or disk definition, Zephyr’s auto-detection fails to turn onDT_HAS_ZEPHYR_FLASH_DISK_ENABLED.
Example of a Correct Setup:
Device Tree fragment (often in boards/*.overlay):
/ {
storage_partition: partition@00030000 {
label = "storage";
reg = <0x00030000 0x00010000>; // Start address and size
};
};
and the supporting prj…
prj.conf example:
CONFIG_FLASH=y
CONFIG_FLASH_MAP=y
CONFIG_FLASH_PAGE_LAYOUT=y
CONFIG_DISK_DRIVER_FLASH=y
CONFIG_FILE_SYSTEM=y
CONFIG_FAT_FILESYSTEM_ELM=y
bottom line… You need to make sure your Device Tree defines a flash partition (label “storage”) and enable the following configs:
CONFIG_FLASH=y
CONFIG_FLASH_MAP=y
CONFIG_FLASH_PAGE_LAYOUT=y
CONFIG_DISK_DRIVER_FLASH=y
Use menuconfig or guiconfig to confirm these.
Also make sure your DTS overlay includes a properly defined storage partition.
HTH
GL
PJ ![]()
Listen to your compiler…LOL ![]()