DFU Virtual USB disk unusable

I’m having the same problem here. Can’t get the DFU USB drive stable enough to do anything. Tried a Windows 8.1 laptop and a Mac MINI… Any clues? And just saying “that’s normal” isn’t gonna cut it. For the life of me, I can’ see why this thing is shipped without the patched BenF firmware… Right now it’s cute, but it won’t be really useful till I can get some new firmware onto it.

To get more specific, under windows 8, the drive may show up for a moment, then the Windows Explorer goes to a scanning/waiting state, and pukes cause the drive can’t be found. The comings and goings cause a bunch of stuff to happen, and always trigger the anti-virus software… On the Mac, the drive comes and goes, and I get a lot of “Disk not ejected properly” notifications… Copy fails with error 43, item cannot be found…

This is very painful!

Edit… To make matters worse, I’m on firmware 4.11. Seems there is no “off” setting on the Ex Data channel, so the hint in this thread to get rid of the purple trace doesn’t work for me… Also, saves of the configuration appear to not take…