Hey, thanks for your reply. Yes I have already deployed the “pet detection” model and it works. But it strugles a bit when it comes to the recognition of cats over middle distances of like than 3m to 7m. I just wanted to try out the “cat detection” model that focuses on cats only.
It is not surprising, but the differences between the models when it comes to distance are really huge sometimes, even for recognizing the same class/object.
Has anyone worked it out with the dedicated “cat detection” model?