Danze Faucet Reviews

Hi there,

The Music Shield is an audio encoder/decoder. It is based on the VC1053B chip, which enabled it to play sound files from SD card and do short-time recording as well.



Pins usage on Arduino



Pins used for Play Control:



D3 - Receiving signal from button for Volume Up.



D4 - Receiving signal from switch for Next Song function.



D5 - Receiving signal from switch for Play&Stop and Record function.



D6 - Receiving signal from switch for Previous Song function.



D7 - Receiving signal from button for Volume Down.



D8 - Green Led instructions.



Pins Used for SPI Interface:



D10 - SPI Chip Select



D11 - SPI MOSI



D12 - SPI MISO



D13 - SPI SCK



Pins Used for VS1053 Interface:



A0 - Reset of VS1053



A1 - Data Require of VS1053



A2 - Data Select of VS1053



A3 - Chip Select of VS1053



We see some one already generate STM32 library for STM32. You can leverage it and compare with our library to do modification. thanks.

<LINK_TEXT text=“https://github.com/rogerclarkmelbourne/ … S1003B_STM”>https://github.com/rogerclarkmelbourne/Arduino_STM32/tree/master/STM32F1/libraries/Serasidis_VS1003B_STM</LINK_TEXT>



Bill