Current leak using a voltage divider with the XIAO ESP32-C6

The sleep current of XIAO_ESP32C6 is 14.3uA. The current consumed by the voltage divider resistor is 18.5uA, which is as small as the sleep current.
However, if we change the way we think about it, connecting a voltage divider resistor doubles the total sleep current to 32.7uA.
If this is a problem, then increase the value of the resistor, or use a voltage divider only when necessary.