Confusion about LoRaWan OTAA via RadioLib on a XIAO ESP32-S3 + SX1262 B2B (-1116)

Hi everyone,

I am working on a project where I’m trying to connect Seeed’s ESP32-S3 + WIO SX1262 sensor node to a paid LoRaWan 1.0.x network. It’s KPN’s (dutch provider) LoRaWan Network in the Netherlands, they claim nationwide coverage. Connecting is only possible with OTAA. Currently the esp32 is connected to WiFi and sends data from a moisture sensor to Arduino Dashboard. The goal is to get the same functionality, but using LoRa technology, as the nodes will be placed in a field eventually without WiFi connection.

They wanted to use KPN’s LoRaWan due to it’s scalability. No P2P connections to a central hub that forwards thbe packets over IP.

Quick unimportant note you can skip:
To be fair, I don’t have much experience with Arduino/Embedded Systems besides one high school project when I was 16. I got this job because I know a bit of C++. Connecting the ESP32 to the Internet was fine, especially with the wiki. But LoRaWan is a whole different story :cry: Maybe partly because getting correct information from ChatGPT when it comes to LoRaWan is near impossible. So i had to do the research myself.

The community posts here helped me a ton and pointed me in the right direction (shout out PJ_Glasso!), like reading the sx1262 datasheet and the fact that LoRa =/ LoRaWan and that I should use RadioLib and some help with the pinouts. But I still have a few questions and I was hoping the community could help me out :))

The problem

I’m consistently failing to join the network. My code uses RadioLib, which returns the error code -1116 during the node.activateOTAA() step. From my research, I believe this means, the esp32s3 is out of range or it didn’t receive a join accept downlink? Now I am in the netherlands, and I live next to a dyke 5 meters below sea level. That could have something to do with it. I don’t know where KPN’s gateways are.

The part that remains confusing for me is what is being handled by RadioLib and what should be handled by me. I’m pretty sure most of the SPI commands and the order in which they should be executed is being handled by RadioLib.

These questions came to mind:

  • ** Is this a range issue? *

  • ** Do I miss something in my code? Like setting tx power?*

  • ** Did I hard-code something that RadioLib already handles?*

  • ** Did I make any mistakes in my setup?*

  • Did I format the DevEUI, JoinEUI, AppKey correctly? I assigned these myself, is that correct?

  • *Is it a power issue? I’m powering the ESP32+sx1262 using the usb port on my laptop/pc. Is this okay to do? *

  • Is it even possible to use the sx1262 for LoRaWan in this way? (Having only the esp32+sx1262, no personal gateways)

  • Is it necessary to both send the uplinks and receive downlinks to start a session? Is that possible with my setup? Can I only send uplinks?

My Code:

Here is the code I’m using for testing the LoRaWan connection. Note: I’m using the pre-configured pinout from the RadioLib Library.


#include <Arduino.h>
#include <RadioLib.h>

// RadioBoards has the B2B pinout of esp32+sx1262
#define RADIO_BOARD_AUTO
#include <RadioBoards.h>

Radio radio = new RadioModule();

// LoRaWAN Credentials + HW COnfig
#define LORA_LDO_EN_PIN 38

// Using placeholder keys for this post.
uint64_t joinEUI = 0x0000000000000000;
uint64_t devEUI  = 0x0000000000000000;
// appkey is 120000...
uint8_t appKey[] = {0x12, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00};
uint8_t *nwkKey = nullptr; 

//  configured for EU868
LoRaWANNode node(&radio, &EU868);

void setup() {
  Serial.begin(115200);
  delay(2000);
  Serial.println(F("LoRaWAN OTAA Join Test"));

  // Power on the LoRa module
  pinMode(LORA_LDO_EN_PIN, OUTPUT);
  digitalWrite(LORA_LDO_EN_PIN, HIGH);
  delay(500);

  // Initialize the radio, this works
  Serial.print(F("Init radio.begin()... "));
  int16_t state = 0;
  state = radio.begin();
  if (state != RADIOLIB_ERR_NONE) {
    Serial.printf("failed, code %d\n", state);
    while (true);
  }
  Serial.println(F("success!"));

  // Start the OTAA join process
  Serial.print(F("Attempting to join lorawan network... "));
  
  //Neccessary to do setRfSwitchPins?
  radio.setRfSwitchPins(38, RADIOLIB_NC);

  // This is the problematic part: always gives -1116
  state = node.activateOTAA(joinEUI, devEUI, appKey, nwkKey);

  if (state == RADIOLIB_ERR_NONE) {
      Serial.println(F("JOIN SUCCESS!"));
  } else {
      Serial.printf("failed, code %d\n", state);
      Serial.println(F("Check keys, range to gateway, and antenna connection."));
      while (true);
  }
}

void loop() {
  Serial.println(F("LoRaWAN Joined successfully. Sending payload..."));
  
  int state = node.sendReceive((uint8_t*)"Hello!", 6);
  if(state == RADIOLIB_ERR_NONE) {
    Serial.println(F("success!"));
  } else {
    Serial.printf("failed, code %d\n", state);
  }

}

Thank you so much for taking the time to read this. Any advice or pointers would be incredibly helpful!!

Best regards,

Ary-x86

OTAA requires receiving the Join Accept → must have bidirectional LoRa link.
If you can only send, you’d need to use ABP (Activation By Personalization) instead—but KPN doesn’t allow that for new devices.

2 Likes

Hi there,

SO , How does it work can you give me/us a 50000’ view of the process? Thanks for the info too. Love those dutch…between the nords, swedes and dutch they have it going ON! :grin:

GL :slight_smile: PJ :v:

Thanks so much for the reply and the encouragement! It means a lot. My initial problem was that I couldn’t figure out which part of this process was failing.

The project is for a client who needs to monitor soil moisture for plants that will be located in a field, outside of WiFi signal. The goal is to do this with the XIAO ESP32-S3 connected to the WIO SX1262 .

The Data Flow will look something lke this:

  • The ESP32 periodically wakes from deep sleep and gets a reading from the moisture sensor.
  • It sends it to a nearby KPN LoRaWan Gateway
  • The gateway forwards it to KPN Things Server, where the data gets decoded and forwarded to an IoT Dashboard, where the client gets live updates.

Now for the big update: I was actually able to send an uplink to the gateway. It was a range issue, as I expected. Now the problem is that I need to receive the JOIN Accept Back from KPN. Now I can see the JOIN Accept downlink is being sent but I still get error -1116. I am quite lost at this stage. I can’t find any information on how to deal with this.

I can’t figure out if it’s a timing issue, or a configuration error.

This is the relevant code snippet currently (I believe some lines are redundant since they’re the default option):

#include <Arduino.h>
#include <SPI.h>
#include <RadioLib.h>

// --- Radio & RF-switch pins ---
SX1262 radio(41, 39, 42, 40);
#define RF_SWITCH_PIN 38
static const uint32_t rfswitch_pins[] = {
  RF_SWITCH_PIN, RADIOLIB_NC, RADIOLIB_NC, RADIOLIB_NC, RADIOLIB_NC
};
static const Module::RfSwitchMode_t rfswitch_table[] = {
  { Module::MODE_IDLE, { LOW   } },
  { Module::MODE_RX,   { HIGH  } },
  { Module::MODE_TX,   { HIGH  } },
  END_OF_MODE_TABLE,
};

// --- LoRaWAN credentials (zeros) ---
uint64_t joinEUI = 0x0000000000000000;
uint64_t devEUI  = 0x0000000000000000;
uint8_t  appKey[16] = { 0 };

// --- LoRaWAN node on EU868, no sub-band filter ---
LoRaWANNode node(&radio, &EU868, 0);

void setup() {
  Serial.begin(115200);
  delay(2000);

  // apply RF switch mapping
  radio.setRfSwitchTable(rfswitch_pins, rfswitch_table);

  // init radio
  if (radio.begin() != RADIOLIB_ERR_NONE) {
    Serial.println("Radio init failed");
    while (true);
  }

  // enable TCXO (1.6 V)
  if (radio.setTCXO(1.6) != RADIOLIB_ERR_NONE) {
    Serial.println("TCXO config failed");
    while (true);
  }

  // prepare OTAA join
  node.beginOTAA(joinEUI, devEUI, nullptr, appKey);

  // join with up to 3 retries
  Serial.println("Joining network...");
  for (int i = 1; i <= 3; i++) {
    if (node.activateOTAA() == RADIOLIB_LORAWAN_NEW_SESSION) {
      Serial.println("Join success");
      return;
    }
    Serial.printf("Join failed (%d), retrying in 30 s...\n", i);
    delay(30000);
  }
  Serial.println("Join failed after 3 tries");
}

void loop() {
  // the rest...
}

Do you have any ideas as to what might be going wrong?
Thanks in advance!

Best regards, Ary-x86