Can't use porcupine with Respeaker Core v2?

Seems like in the Readme of the porcupine github repo it states that it supports following platform:

cross-platform:

Arm Cortex-M, STM32, Arduino, and i.MX RT
Raspberry Pi, NVIDIA Jetson Nano, and BeagleBone
Android and iOS
Chrome, Safari, Firefox, and Edge
Linux (x86_64), macOS (x86_64, arm64), and Windows (x86_64)

where our ReSpeaker Core v2.0 is based on Rockchip RK3229, a quad-core ARM Cortex A7 platform. So I guess this processor has not been tested with the picovoice team and that’s why they state that they do not support this platform.

If you willing to give it try that will be great, I would suggest to show some error logs so that the people who are also interest can debugging with you together.
Thanks