Seeed Studio Forum
Can the XIAO nRF52840 do BLE Mesh?
Products & Technology
XIAO
PJ_Glasso
February 16, 2023, 4:48am
4
20221029_113813
1920×1920 183 KB
20221029_113831
1920×1920 163 KB
20221029_113856
1920×1920 144 KB
20221029_113950
1920×1920 160 KB
The Secret is in the POGO pins…
20221029_201335_Moment
1440×1440 138 KB
Even on the dev board, they terminate into the two row of pins you see connected to the adapter board for the jlink plus.
Debugging in Platform IO and vscode works well. Haven’t got Arduino Debug to go though.
HTH
GL
show post in topic