Can I use IMU sensor (MPU9250) with Wio Terminal?

^^ I already mastered the internal IMU sensors ^^
please see my video for this ^^ : https://youtu.be/XAQ2tjaLBfI

My task is to compare two IMU sensors one is internal in Wio Terminal and the other is the grove sensor (from Seeedstudio)

the codes are just the example codes like the followings;
and the only problem occurred while including “I2Cdev.h”

===============================================================

#include “Wire.h”
// I2Cdev and MPU9250 must be installed as libraries, or else the .cpp/.h files
// for both classes must be in the include path of your project
#include “I2Cdev.h”
#include “MPU9250.h”
// class default I2C address is 0x68
// specific I2C addresses may be passed as a parameter here
// AD0 low = 0x68 (default for InvenSense evaluation board)
// AD0 high = 0x69
MPU9250 accelgyro;
I2Cdev I2C_M;
uint8_t buffer_m[6];

int16_t ax, ay, az;
int16_t gx, gy, gz;
int16_t mx, my, mz;

float heading;
float tiltheading;
float Axyz[3];
float Gxyz[3];
float Mxyz[3];

void setup()
{
// join I2C bus (I2Cdev library doesn’t do this automatically)
Wire.begin();

// initialize serial communication
// (38400 chosen because it works as well at 8MHz as it does at 16MHz, but
// it's really up to you depending on your project)

Serial.begin(38400);

// initialize device

Serial.println("Initializing I2C devices...");
accelgyro.initialize();

// verify connection
Serial.println("Testing device connections...");
Serial.println(accelgyro.testConnection() ? "MPU9250 connection successful" : "MPU9250 connection failed");
delay(1000);
Serial.println("     ");
//  Mxyz_init_calibrated ();

}

void loop()
{
getAccel_Data();
getGyro_Data();
Serial.printf("%4.2f %4.2f %4.2f %4.2f %4.2f %4.2f\n",
Axyz[0], Axyz[1], Axyz[2], Gxyz[0], Gxyz[1], Gxyz[2]);
delay(10);
}

void getAccel_Data(void)
{
accelgyro.getMotion9(&ax, &ay, &az, &gx, &gy, &gz, &mx, &my, &mz);
Axyz[0] = (double) ax / 16384;
Axyz[1] = (double) ay / 16384;
Axyz[2] = (double) az / 16384;
}
void getGyro_Data(void)
{
accelgyro.getMotion9(&ax, &ay, &az, &gx, &gy, &gz, &mx, &my, &mz);
Gxyz[0] = (double) gx * 250 / 32768;
Gxyz[1] = (double) gy * 250 / 32768;
Gxyz[2] = (double) gz * 250 / 32768;
}