CAN-BUS Error 5 and solid INT LED

Hello guys i have the same problem i have a can bus shield v1.2 and a opel astra car, if i only want to receive data it works fine, when i try to send data the checkerror() it show 0 0 then 5 CAN_CTRLERROR. Can someone please help me? Almost forgot i use a arduino uno and the SPI_CS_PIN = 9;