Hello,
and I’m sorry I’m so late to the party, but I’ve been looking around and couldn’t really find any LiPo charging module that would allow the following:
On the Rider Plus, is it possible to carry the D+/D- lines from the USB-C socket over to the USB-A socket? Maybe even as a one-off hack?
What I have in mind is an upgrade to my portable turntable, which I’m building using off-the-shelf parts. Basically I put a small LiPo battery into an existing MTT1 turntable. my battery output goes to a boost converter to generate the 9V I need for the motor / original circuitboard and to a headphone amplifier via a B0505S-1W 5V-5V Isolated Module (which does work when fed 4.2V instead of 5V).
As an upgrade, I would now like to use a Behringer U-Phono UFO202 USB soundcard as the phono preamp (I have tested this, the sound card works as a phono preamp when simply connected to a USB charger). So on the Rider Plus, I would connect it to the USB Type A socket.
However, if the Rider Plus could work as a USB data passthrough (at USB 2.0 speeds) as well as a LiPo charging board, I would then be able to connect my portable turntable to my Android mobile phone using an OTG cable and use the UFO 202 as a soundcard to record vinyls on the go. This is something I have tested separately using AudioRecorder (no ads) which works really well.
Any advice welcome, thank you