Yes, the elf format is not important. The “real” binary content gets stripped out of the elf file into the bin (or dfu) file, which gets loaded on the Nano. So whether the intermediate format is elf or ubrof does not matter.
Exactly this issue should be fixed by the patch I suggested in viewtopic.php?p=4498#p4498. Basically the patch makes the LIB do the same when jumping to the APP, as the bootloader does when jumping to the LIB: It reads the startup entry (reset handler) from the interrupt vector instead of using a hardcoded address of the startup entry.
I have tested the patch on an emulator, so I know that it compiles correctly and does the right thing. However, I can not see if it works on gcc, so I will need some of you to please test it on IAR 4.0 and 5.0.