build your own cross-compiler !!!

Yes, this is how it is. The git tree I am playing with is basically the 2.5 APP. It uses calls to the closed source 2.5 LIB. If the LIB was open-source I would have put it inside the git tree, and we would not have so much trouble with the lib function calls, which I think is the reason it does not work. On the other hand, the 1.1 source was from before the split into APP and LIB (originally to overcome the IAR 32k limitation). So maybe that would have been an easier start.

Theoretically it should be possible to recompile the 2.5 APP with gcc (from my git tree) and use it together with the 2.5 LIB. But there are some issues, maybe from calling IAR-compiled code from gcc-compiled code. I think there are some bugs in gcc also, dealing with cortex-m3, for instance the thumb/arm wrappers which should not be there since the cortex-m3 is thumb only.

On your DSO Nano, the bootloader runs at 0x0800000. As long as you do not want to upgrade (pressing the down button) it jumps to the LIB code, which starts at 0x08004000. After displaying the LIB version, it jumps to the APP code which starts at 0x0800c000. In the APP code there are various calls to functions in the LIB.

Each APP hardcodes the addresses of functions in the LIB. So any APP depends on a particular version of the LIB. The LIB has a function vector table so it can be recompiled without having to change the APP again, I suppose. But the ABI (application binary interface) has to match, with a precise definition of what each function does and returns and the number and type of arguments.