Okay some commented that I had an other device connected, and I have always seen that print out, but if I do it is builtin to this Mac.
If I unplug everything I still see the line
Found Runtime: [0x05ac:0x8216] devnum=4, cfg=0, intf=3, alt=0, name=“UNDEFINED”
I had assumed this was normal. If I connect the DSO it appears as two devices the
Found Runtime: [0x0483:0xdf11] devnum=4, cfg=0, intf=0, alt=0, name="@Internal Flash /0x08000000/12001Ka,116001Kg"
Found Runtime: [0x0483:0xdf11] devnum=4, cfg=0, intf=0, alt=1, name="@SPI Flash : M25P64/0x00000000/64064Kg,64064Kg"
both of which I see on a PC. Am I confused, highly likely. or is something else going on?