build your own cross-compiler !!!

Using the binary I built from the tarball it is still claiming to download the full firmware, so I think the bootloader is still there. Can someone send me the full set of commands I need to use to download the firmware to get up again? The device says it is a DSO Nano v1.1
DS0201 Device Firmware Upgrade Ver 2.0

I have only tried downloading the lib and app, both the 2.1, 2.5, and 3 versions. One of the times I must have done it okay, but now I am not hitting on the right version to be functional again.