Jerry, that’s really Great! What’s needed in order to submit code?
__APP_Start is exported from LIB, so if you instruct IAR5 to generate a .map file (think objdump -x in gcc jargon) you will find its address in it. The pointers table is then easy to build - just add 4 bytes of offset for each pointer:
address of __USB_Instr -> address of __APP_Start + 4
address of __CTR_HP -> address of __APP_Start + 8
...
Maybe that part could also be done explicitly, defining a symbol __App_Start_address in APP that knows the address of __APP_Start in LIB (which should really be set explicitly by configuring the linker, as I was saying above) and then using it to express the needed function addresses.
Antonio