This feature would provide the greatest benefit to those who need glasses but hate to wear them all the time. For ease of use they simply select Vpp for DC volts, Vrms for AC volts, Freq for frequency, etc.
Possible food for thought to implement this feature with minimized code impact. Because the present ME menu already displays the measurement selected at last pop-up at the top right of screen, it might be possible to add a “meter visible”/“meter hide” option on the ME pop-up menu. When the pop-up closes, the larger characters of the selected measurement value would overlay the screen (“meter visible”) and also still remain at it’s normal location (top right of screen). If they mistakenly close the ME pop-up with “meter visible” selected, then display “Select” for the ME results.
“Meter hide” would operate as it does now with no large characters.
If you used the same magenta color of the oversize characters as the waveform color, then the waveform could still update on the screen with minimal interference with the block style large characters. Otherwise you could just disable the waveform updates during “meter visible” mode.