Hi ,Smartlscar:
I don’t think I can support you on this issue, but I can offer some suggestions about Battery charging and XIAOnRF52840:
when using XIAO nRF52840 (Sense) for battery charging。When P0.14 (D14) turns off the ADC function at a high level of 3.3V, P0.31 will be at the input voltage limit of 3.6V. There is a risk of burning out the P0.31 pin.
Currently for this issue, we recommend that users do not turn off the ADC function of P0.14 (D14) or set P0.14 (D14) to high during battery charging.