The final circuit has been built inside the phone enclosure, including amplifiers for the speaker and the microphone. Playback and record modules are developped an tested but the application code only supports playback for the moment.
speakers uses white noise to monitor the breathing and movement of sleeping babies. Developed by researchers at the University of Washington, BreathJunior plays the noise from the device and then records how it is reflected, in order to detect the tiny motions made by infants’ chests as they breathe. It can also pick up the sound of crying.