I already updated my Mic Array to the 1 channel firmware.
So does this mean there is no plan to raise the audio output quality / sample rates?
This would mean the mic array would always provide very poor audio output (even on good speakers).
The WM8960 Audio Chip on the Mic Array can handle these Samplerates: 8, 11.025, 12, 16, 22.05, 24, 32, 44.1, 48 KHz
The XVF3000 Chip can handle Samplerates: Up to 48kHz sample rate
Just for comparison:
ReSpeaker MicArray v2 Quality - 16 KHz/24 bit
CD Quality - 44,1 KHz/16 bit
DVD Quality - 48 KHz / 16 bit
Hi-Res Audio Quality - 96 kHz/24 bit
Studio Quality - 192 KHz/24 bit
UPDATE: Bill I think you misunderstood me, I’m talking about audio output (speaker) not audio input (microphones)