Arduino Mega 2560 + BT Shield

Hi Steve,



I’m trying to connect the Bluetooth Shield with the Mega 2560 and I’m a little bit confuse, is the connection in the following image correct?



<LINK_TEXT text=“http://www.seeedstudio.com/wiki/File:Bl … a_2560.jpg”>http://www.seeedstudio.com/wiki/File:Bluetooth_connect_with_Mega_2560.jpg</LINK_TEXT>



Are you connecting the Tx1/Rx1 of the Mega 2560 to the Rx/Tx of BT Shield? It seems that you are connecting them to 0/1 pins of the Mega 2560, aren’t you? The correct would be to use the BT_RX/BT_TX lines, wouldn’t it?



Please, could you clarify this issue?



Congratulations for your good work.



Best regards,