The water pump I have selected outputs RPM signals similar to a standard three wire PC fan. In fact you can plug the signal wire to the CPU fan header on a motherboard and if your pump dies or stops sending a signal it will shut your PC down to prevent a CPU failure due to heat. While a nice feature for safety, it will be much cooler to see the RPM at which your pump is running than knowing your CPU wont melt if it dies right?
Since the Fan and Pump RPM signals are so similar, and my water pump has not arrived yet I decided to dev using a 120mm PC fan. The following schematic should explain how to wire things up.
[CENTER][/CENTER]
This is pretty simple to hook up. First you need to run the Signal wire (almost always yellow) to the breadboard. Then from it connect a jumper wire to Arduino Digital Pin 2. Also from the sensor wire you need to connect a 10k resistor to the Arduino’s 5V pin. This is a simple pull-up resistor. We also need to make sure that we connect the fans ground line to one of the Arduino’s ground pins. Next just connect the fans power wire to the PSUs 12v line and the fans ground wire to the PSUs ground.
Now upload the following code to your Seeeduino, and then open the serial terminal. Again I would like to thank Crenn from thebestcasescenario.com for his help figuring out the code. Please note that this code will change in the final part of the project. The Fan / Pump RPM will be displayed on the LCD from the first post in this thread.
[code]//code by Crenn from http://thebestcasescenario.com
//project by Charles Gantt from http://themakersworkbench.com
/*To disable interrupts:
cli(); // disable global interrupts
and to enable them:
sei(); // enable interrupts
*/
//Varibles used for calculations
int NbTopsFan;
int Calc;
//The pin location of the sensor
int hallsensor = 2;
typedef struct{ //Defines the structure for multiple fans and their dividers
char fantype;
unsigned int fandiv;
}fanspec;
//Definitions of the fans
fanspec fanspace[3]={{0,1},{1,2},{2,8}};
char fan = 1; //This is the varible used to select the fan and it’s divider, set 1 for unipole hall effect sensor
//and 2 for bipole hall effect sensor
void rpm () //This is the function that the interupt calls
{
NbTopsFan++;
}
//This is the setup function where the serial port is initialised,
//and the interrupt is attached
void setup()
{
pinMode(hallsensor, INPUT);
Serial.begin(9600);
attachInterrupt(0, rpm, RISING);
}
void loop ()
{
NbTopsFan = 0; //Set NbTops to 0 ready for calculations
sei(); //Enables interrupts
delay (1000); //Wait 1 second
cli(); //Disable interrupts
Calc = ((NbTopsFan * 60)/fanspace[fan].fandiv); //Times NbTopsFan (which is apprioxiamately the fequency the fan is spinning at) by 60 seconds before dividing by the fan’s divider
Serial.print (Calc, DEC); //Prints the number calculated above
Serial.print (" rpm\r\n"); //Prints " rpm" and a new line
}[/code]
You should see an RPM output in the serial terminal. It is accurate within 10-15 RPM of the fans actual RPM which is close enough for me. If your RPM output seems to be double what it should be your fan may have a bipolar Hall efect sensor and its counting each pass of the magnets pole as a single RPM when each should be 1/2 an RPM. No worries though as this is an easy fix. Just simply change the " char fan = 0 code from 0 to 1. Upload the modified code and you should be seeing accurate RPM numbers.
Next time we will cover how to measure and display the liquid flow rate of the system.
What I have left to do:[/SIZE]
- Work out flow meter design and schematic
- Determine alarm parameters
- Complete code and refine it.
My fritzing page on this project.(Download all the files there)
Reading PC Fan / Water Pump RPM with an Arduino