Any chance of reloading the firmware under OSX or Linux

Well, the DSO is actually a STM32 device. So if anyone wants to venture onto an STM32 enthusiast forum and ask how to flash firmware in DFU under Linux (OS X is probably similar) then it would help us adapt it to the DSO. I wonder if there is a generic protocol for it or if DeFuSe is proprietary…