That makes sense, thanks!
It looks like the FreeCAD file on the REV2 Thingiverse page is for an older revision of the part. Do you mind uploading the latest FreeCAD file?
I’ve run into a couple issues with this breakout board:
- The debug pogo pins seem to be in the wrong spot? They don’t seem to be making an electrical connection. I think they need to be moved about 0.9 mm up (i.e. in the direction of the USB-C port).
- The holes that the bent pins go into are too small (they’re smaller than the other set of “mounting” pin holes).
I’d be happy to help fix these issues if you could upload a new version of the file