Salman
Thank you for your response. I have already done everything you suggest.
I have attempted to run the program again this morning
This is a copy of the responses.
The program seems to list the help information but will not accept the command
./amebad_flash_tool erase --port COM8
PS C:\Program Files\amebad_flash_tool_v0.1.0_windows> ./amebad_flash_tool
Usage: amebad_flash_tool.exe [OPTIONS] COMMAND [ARGS]…
RTL872XD Flash tool
This tool is used to burn rtl8720d firmware.
Options:
–version Show the version and exit.
–help Show this message and exit.
Commands:
erase
flash
PS C:\Program Files\amebad_flash_tool_v0.1.0_windows> ./amebad_flash_tool erase --port COM8
Erasing…
‘C:\Program’ is not recognized as an internal or external command,
operable program or batch file.
done!
PS C:\Program Files\amebad_flash_tool_v0.1.0_windows>
Thanks for your help.
Allan