BoRRoZ
I was confident that I had done that but I have gone through the process again.
I went into bootloader mode and the D:Arduino window popped up. I dragged the file into the window; I saw it momentarily on the file list and then it rebooted.
I went back into bootloader mode and the file was no longer there.
I tried the amebad program agian - but I still get the same error.
PS C:\amebad_flash_tool_v0.1.0_windows> .\amebad_flash_tool erase -p COM9
Erasing…
error: Enter Uart Download Mode
Image tool closed!
done!
PS C:\amebad_flash_tool_v0.1.0_windows>
Any further thoughts would be appreciated.
Allan