Alternative dso firmware [Application Software Design Entry]


I don’t understand why you are using the -march=armv7 option. It should be enough to specify -mcpu=cortex-m3 which already defines the architecture. Also. the architecture for the cortex-m3 used in STM32F103 is armv7-m and not armv7. Possibly your conflicting architecture specification fools the toolchain into allowing ARM instructions.


You can see all instructions in the .plt section are 4 bytes wide, a typical sign of ARM instructions and not Thumb. This is the root of your problem: The toolchain has compiled and labelled this code as ARM code and therefore also calls into it with pair addresses (like 0x200050cc, or 0x200050e0 in your other post).