Alternative dso firmware [Application Software Design Entry]

Hello gabonator1,


Regarding the completion degree of your firmware, maybe there is a confusion because you write



[size=85]Todo list:

finish oscilloscope module - 92% done

calibration - 80% done

fft view - 80% done

signal generator - 90% done

connection with android tablet/phone - 90% done

optimize ROM usage (many bitmaps are stored as 8bits per pixel) - 0%

[/size]

… but to be honest, I didn’t notice anything not working…



There is a function which I would love: the ability to display alle 4096 samples at once by default (i.e. a complete sweep) and to be able to zoom in (a factor 16 = 4096/256 shoud be possible). Of course, this would not work for the shortest time bases. Maybe this is what is called oversampling. Or is it already implemented and I didn’t find it?



Anyways, I congratulate for your fantastic work, thank you!

Patrick