Joined the forum specifically to thank you gabonator !
I received my DS203 the other day and was perplexed by the Factory firmware. After a quick bit of searching your name kept popping up, so I took a look here, liked the ‘lifestyle’ type of easy on the eye look to your firmware and the functions. Plus, that you obviously spend a heck of a lot of time on the project. Installed it, ran it and the DS203 was scoping away til I thought to charge the battery !
Again, thanks so much…brilliant work !
As a bug report and hopefully useful bit of info not crtiticsm…the Square wave in the generator seems to often start with a display of 36MHz, but then will drop down as though at the 9MHz top speed. It goes straight into the 8MHZ ranges from that errant 36MHz.
Also, I noticed a spelling mistake on one screen, will try to find again, but something small like ‘triger’ instead of ‘trigger’.