I only used the available models. For example, counting people. We could expect there to be feedback on the number of people seen, sent with LoRa.
There is no information on the number of people. Just information on the model used.
We are waiting for support to be able to retrieve information via LoRa. Our goal is to count the number of bikes on a cycle path, retrieve the partial total every hour in order to make a count throughout the year with an autonomy of the whole of several months as indicated on the site.
The best is to put on the web side “Product in beta version” as the result is not what people expect.
We are using other product like LoRa gateway and not problem with it.
I am keeping hope for the A1102 product which can a great product as the wiki explain