I was able to get two to see each other with the stock firmware (2.4.0 came on these) and latest iOS Meshtastic app. I do see some ‘oddities’, not sure if it is the app. One app does not seem to show the second device on the map, but it is listed in the node page. Devices are sitting about 2ft apart, so distance did not cause a problem here. It seemed like I had to wait about 30 seconds for initial connection between the two, but that might have been me being confused about the lack of map display for one device on the iPhone.