The linked firmware won’t even boot on my ReSpeaker Core v2.
At power up I get a green light, followed by activity on both blue lights, a single blink of three red lights near mics 2,3,4 on the back of the board – then the cycle just repeats. I get no serial port presented on the OTG connection and no network on my wired ethernet port.
Hi, we optimized more than 60% of code from uboot to kernal to improve the performance on the new image. We suggest change to new firmware. thanks for understanding.
Any chance there is a “flasher” image of this version of the OS?
I have been able to find a earlier versions on your various one drive/google drive/random other locations that the docs point you to, but have as of yet found one for the 20180610 version.
WARNING: While this looks like it should work it doesn’t
Looks like any image can be made a ‘flasher’ image simply by booting from the sd card with the image you want written to it (either iot or lxqt) and then running /opt/scripts/init-eMMC-flasher-respeaker.sh as root…
Thats all the image builder script does when it creates a flasher image. It just auto executes that script on boot.
This also exposes a nice way to create an “image” easily. Just boot from the SD card, do all your work to get it the way you want, and then use it to flash each respeaker you want.
UPDATE: Just did that on one of my core v2’s and sadly while the script runs, and it looks like it works, it doesn’t result in a bootable device after the fact.
So I’ll stick to booting off a SD card for now, as all the flasher images don’t actually have working a GPIO pin for the LED enable pin.
And my question still stands Seeed. Is there a more update to date functional flasher image?