reServer i51135 RAM?

So I just bought the reServer i51135 and none of the RAM is available to buy here. Does it come with ram or do I have to buy the RAM elsewhere? If I buy RAM elsewhere can it use standard DDR4(3200) laptop ram?
I was thinking about getting the “G.SKILL Ripjaws Series 32GB (2 x 16GB) 260-Pin DDR4 SO-DIMM DDR4 3200 (PC4 25600) Laptop Memory Model F4-3200C22D-32GRS” if it will work and if it doesnt come with RAM already. Will that work with it?

Yes, it works. :smiley:

1 Like

Sweet. Thank you very much!