Seeeduino Lotus error when uploading

Arduino, Seeeduino Serials and mutants. Share your problems and experence on arduino compatible board such as seeeduino/stalker, etc.

Moderators: lily.li, violet, salmanfarisvp

Post Reply
r0b0tn1k
Pre-kindergarten
Pre-kindergarten
Posts: 5
Joined: Fri Apr 27, 2018 3:13 am

Seeeduino Lotus error when uploading

Post by r0b0tn1k » Wed Jan 23, 2019 6:31 am

I have a new PC and I cannot get the Seeeduino Lotus to work. It worked fine on my last pc.

I installed the drivers, and when I try to upload, I get error:
No device found on cu.SLAB_USBtoUART
An error occurred while uploading the sketch

I have selected Seeeduino Lotus - Cortex - M0+ as the board.

Port is /dev/cu.SLAB_USBtoUART

Programer is AVR ISP.

It does not allow me to select baud rate or other information, I only have Board and Port for this board.

I tried uploading to NodeMCU and that works, so the driver is ok.

Please advise.

bill.yu
Junior-7
Junior-7
Posts: 707
Joined: Mon Apr 02, 2018 11:05 am

Re: Seeeduino Lotus error when uploading

Post by bill.yu » Thu Jan 24, 2019 2:29 pm

Hi there,

Seeeduino Lotus 1.0 works at Windows Operating System ONLY. Seeeduino Lotus 1.1 works with Window and Mac.

which version do you have? thanks

r0b0tn1k
Pre-kindergarten
Pre-kindergarten
Posts: 5
Joined: Fri Apr 27, 2018 3:13 am

Re: Seeeduino Lotus error when uploading

Post by r0b0tn1k » Fri Jan 25, 2019 8:49 pm

Hi, I have 1.1 version. I can provide photo for proof if needed.

Post Reply