LTE Cat 1 Pi HAT - Further steps and APN

Applications/questions using Raspberry Pi with Seeed products, please post it here.

Moderators: lily.li, violet, salmanfarisvp

Post Reply
vishwaspowar235
Pre-kindergarten
Pre-kindergarten
Posts: 1
Joined: Tue Sep 25, 2018 2:22 am

LTE Cat 1 Pi HAT - Further steps and APN

Post by vishwaspowar235 » Tue Sep 25, 2018 2:47 am

Hi,

I have used the LTE Cat 1 Pi HAT shield for US carriers both AT&T and VERIZON using the Hologram sim. This hologram sim otherwise connects to Verizon or AT&T signal based on the available network. I have following questions:

1. Will I require to configure APN ? If yes which file or AT commands can I use for that purpose?

2. I followed the steps given here: [/http://wiki.seeedstudio.com/LTE_Cat_1_Pi_HAT/], I did get all the output as expected, with RSSI 7. But I still cannot to the internet, is there another script to keep it connected to the internet? Will I get a static IP after connection? Basically what is to be done next?

Best,
Vishwas

bill.yu
Junior-7
Junior-7
Posts: 702
Joined: Mon Apr 02, 2018 11:05 am

Re: LTE Cat 1 Pi HAT - Further steps and APN

Post by bill.yu » Fri Nov 02, 2018 5:53 pm

Hi Vishwas

We are writing the APN examples and will update the wiki later on. thanks.

Post Reply