Firmware 1.5

Moderators: lily.li, violet, jeremy882, crail.lyu969

brianez21
Pre-kindergarten
Pre-kindergarten
Posts: 11
Joined: Thu May 27, 2010 12:29 pm

Re: Firmware 1.5

Post by brianez21 » Mon May 31, 2010 10:32 am

Paul2 wrote:SE settings: vertical stalls, stalls level, multiple probe,
Click the up and down, left and right gear to achieve vertical and horizontal adjustment of stalls;
Long by up and down, left and right position adjustment to achieve;
Long press M button to select multiple probes;
Play starts scanning short or suspended by scanning
Press and Play show or hide all measurements.

MO Set: Scan mode, trigger mode,
Select trigger mode by up and down, left and right select the scan mode;
Short press Play to the SE menu


Tr settings: trigger level, trigger sensitivity,
Adjusted by the upper and lower trigger level, so adjust the trigger sensitivity.
Press and M blanking trigger line;
Short press Play to the MO menu
Press and Play directly to the SE menu.

C1 set: cross cursor 1 position
Cursor up and down to adjust the level by 1, so adjust the vertical cursor 1.
M blanking press and move the cursor to the previous instructions on the values -> blanking on the last move of the cursor and the direction value -> display the last move of the cursor on the values and instructions;
Short press Play to Tr menu
Press and Play directly to the SE menu.

C2 settings: Cross 2 cursor position
Cursor up and down to adjust the level by 2, so adjust the vertical cursor 2.
M blanking press and move the cursor to the previous instructions on the values -> blanking on the last move of the cursor and the direction value -> display the last move of the cursor on the values and instructions;
Short press Play to C1 menu
Press and Play directly to the SE menu.

Me Select: measurement mode, set the measurement display mode,
Selected by measuring the content of the upper and lower,
Long right-click shows all measurements,
Long press left hidden;
Short press Play to C2 menu
Press and Play directly to the SE menu.

Of set: x-axis offset, y-axis offset,
Press down to adjust the vertical offset, so adjust the level of migration.
M blanking offset by the level of long reference line;
Short press Play to Me menu
Press and Play directly to the SE menu.

Fo settings: the output pulse frequency
Short-pulse frequency by up and down to adjust the output gear, press down to adjust the output accounted for aspect ratio;
Short by about fine-tune the output pulse frequency, long pulse output by about coarse frequency;
Of the short press Play to the menu
Press and Play directly to the SE menu.

FL: file operations,
Right click choose save, left click to select the reading, press down the selection process number, press M the implementation of selected operations;
Long press the button down, move the location of reference waveform,
Long press the left button, hidden reference waveform,
Long press the right button to display the reference waveform.
Short press Play to Fo menu
Press and Play directly to the SE menu.


Time does not operate automatically return to SE menu.


Save method parameters: Set a good start after at least 5 minutes to ensure, or can be non-SE menu press and hold PLAY button until prompted;
Hold down the M key to boot, you can use the default settings.


Time increment between two time the cursor into the frequency display: C1 or C2 in the menu click the down button can display time, display frequency,
Automatically switch between three modes alternately.


Voltage correction to use:
a) zero correction
Hold down the left-turn, short the probe, open the measurement display. Press down button to select the correct short-stalls, short press the left or
Right to show the average voltage closest to 0V.
b) Gain correction
Prepare a reference power, hold down the right boot, then the probe base power, open the measurement display. Press down button to select short
Correction of stalls, short press the left or right to display the average voltage closest to the reference power value.
To achieve the best results, repeat this process several times, complete short press M key once, then press and play button to save. Hold down the M key if
Boot, will not use the saved calibration data.


To avoid the slow USB charging oscilloscope display, the normal boot will be shielded USB communications, PC will be displayed at this time does not recognize the USB device,
To use USB communications, press and hold the M key to boot.

Hold down the Play button start, the Play button function with the V1.4 version.
^ Google translation from Chinese

User avatar
esp
Elementary-3
Elementary-3
Posts: 361
Joined: Fri Aug 22, 2008 5:45 pm

Re: Firmware 1.5

Post by esp » Mon May 31, 2010 2:43 pm

Paul's Firmware 1.5 operation manual.
Translated by Eric Pan from Seeed Studio 5/31/2010

Basic operation:
Press M to switch cycle downwards around menu items.
Press R/S to switch cycle upwards around menu items.
Press R/S and hold to jump back to Se (basic measurement) menu.
Use direction keys to adjust.
After long time idle, firmware jumps back to Se menu

Save parameter:
Keep power for 5 minutes for latest setup, or press and hold R/S button for menu other than Se.
Press M while powering up to use factory setting.

Frequency/Time measurement change.
Press UP/DOWN under C1 or C2 menu to toggle among Time/Frequency/Auto switch

Calibration
a) Zero calibration
Press LEFT while powering up, connect black and red probe. In Se menu, Press UP/DOWN to choose scale needs calibration, press LEFT/RIGHT to adjust the displayed average voltage to 0V.
b) Gain calibration
Prepare a reference power source, press RIGHT while powering up, attach probe to reference power supply. In Se menu, press UP/DOWN to choose the scale needs calibration, press LEFT/RIGHT to adjust the displayed average voltage to the power source.
To get the best result, please repeat above processes, press M after completion, then press and hold R/S to save to parameter.

USB communication
When connected to PC, USB communication is disabled by default, PC will report unrecognizable USB device.
To use USB communication, please press M while powering up.

================================Menu operations as below======================
Se Menu:
To set vertical Scale, Time Base, Probe attenuation scale
Press UP/DOWN to adjust vertical scale, Press LEFT/RIGHT to adjust time base
Press and Hold directions to adjust waveform positions
Press M to switch probe attenuation scale
Press R/S to run and stop waveform
Press and hold R/S to display or hide all measurement items.
Mo Menu:
To set scan mode and trigger mode
Press UP/DOWN to choose trigger mode, Press LEFT/RIGHT to choose scan mode

Tr Menu:
To set trigger level and trigger sensitivity
Press UP/DOWN to adjust trigger level, LEFT/RIGHT to adjust trigger sensitivity
Press and hold M to display/hide trigger level marker

C1 Menu:
To set cross cursor 1 (Red dotted lines)
Press UP/DOWN to adjust horizontal cursor 1, Press LEFT/RIGHT to adjust vertical cursor
Press and hold M to toggle display of latest modified cursor and value

C2 Menu:
To set cross cursor 2 (Blue dotted lines)
Press UP/DOWN to adjust horizontal cursor 1, Press LEFT/RIGHT to adjust vertical cursor
Press and hold M to toggle display of latest modified cursor and value

Me Menu:
To set measurement mode and display
Press UP/DOWN to set measurement mode
Press and hold RIGHT to display all measurement items
Press and hold LEFT to hide

Of Menu:
To set horizontal position and vertical position
Press UP/DOWN to adjust vertical position, Press LEFT/RIGHT to adjust horizontal position
Press and hold M to toggle display of horizontal indicator

Fo Menu:
To set output waveform characteristics
Press and hold UP/DOWN to adjust duty cycle
Press UP/DOWN to adjust frequency in rough stages
Press LEFT/RIGHT to tune frequency in 1% scale
Press and hold LEFT/RIGHT to tune in 10% scale

FL Menu:
To operate file on SD card
Press RIGHT to save, Press LEFT to load, Press UP/Down to select #, Press and hold M to execute.
Press and hold UP/DOWN to move reference form
Press and hold LEFT to hide reference waveform
Press and hold RIGHT to display reference waveform

Tried to translate here. Please let me know if anything mistaken. thanks!

BenF
Elementary-2
Elementary-2
Posts: 231
Joined: Mon Nov 23, 2009 1:01 am

Re: Firmware 1.5

Post by BenF » Mon May 31, 2010 3:24 pm

Excellent! :)

I think the above post is worthy of a PDF available for download from the repository (perhaps even an editable word source so others can add to it).

I still have a couple open questions :

- Is the SINGLE trigger mode working (continues sampling with no screen update until trigger)? How do I restart scanning for the next trigger event?
- How can I stop/start sampling (freeze the display in any trigger mode) and then pan screen left/right to see more of the captured waveform?

peterjohnston
Pre-kindergarten
Pre-kindergarten
Posts: 17
Joined: Mon Feb 08, 2010 3:47 am

Re: Firmware 1.5

Post by peterjohnston » Mon May 31, 2010 9:20 pm

Don't know about anybody else but I'm having trouble changing the vertical scale using the "up" button in "Se" mode. I can move the waveform up and down by holding it as described, but just pressing up doesn't reduce the volts/division.

Edit: I've got hardware v1.1.

Edit 2: The "up" button needs pressed several times in any mode to register it. Is it polled or does it use an interrupt?

User avatar
esp
Elementary-3
Elementary-3
Posts: 361
Joined: Fri Aug 22, 2008 5:45 pm

Re: Firmware 1.5

Post by esp » Wed Jun 02, 2010 10:27 am

Maybe something jamming the up button?

micha-uhl
Pre-kindergarten
Pre-kindergarten
Posts: 7
Joined: Thu May 06, 2010 11:10 pm

Re: Firmware 1.5

Post by micha-uhl » Sat Jun 05, 2010 12:05 am

Thank you, Paul! Very good. The DSO becomes better.

kamisama
Pre-kindergarten
Pre-kindergarten
Posts: 8
Joined: Tue Jun 15, 2010 11:32 am

Re: Firmware 1.5

Post by kamisama » Tue Jun 22, 2010 10:55 am

Paul, your firmware is the best, but you can include LOGOS to reeplace seedstudio, dso nano... originally my DSO shows e-design. when I try some firmwares I lost it.

davidea
Pre-kindergarten
Pre-kindergarten
Posts: 6
Joined: Tue Jul 13, 2010 5:20 am

Re: Firmware 1.5

Post by davidea » Mon Jul 19, 2010 1:33 am

entusiast about this project, i've made a brief discussion on it and a manuals' italian translation


http://www.davidea.it/elettronica/45-va ... o-201.html

i'm not a professional translator, then if someone find error , please tell me!

piccola recensione e traduzione italiana del manuale, liberamente utilizzabile da chiunque! segnalatemi eventuali errori ed inesattezze.

Syberian
Pre-kindergarten
Pre-kindergarten
Posts: 1
Joined: Wed Sep 22, 2010 10:19 am

Re: Firmware 1.5

Post by Syberian » Wed Sep 22, 2010 12:02 pm

Hi guys!
I want to share my experience with the DSO nano here.

Just a two days ago I have received one from ebay. It was flashed with the latest Paul 1.5.20 firmware. So everything was ok but the voltage readings was biased with +800mV.
Seeed firmware has no gain and zero adjustments. Paul`s one wont write to microSD its settings.
The 2nd way was more clear so I have started my little research.

Here`s the results.

To have an opportunity of using the microSD card with Paul 1.5 do the following step-by-step:

1- Get an microSD 2GB card (do NOT buy Kingston!). I have Apacer 2GB working good. Maybe you should switch between several vendors.
2- Put the card into the card-reader or notebook and format it in FAT (FAT16) with standard cluster size.
3- Put it in the DSO Nano
4- power the DSO up while holding the M button. Do NOT use any DSO functions to not ruin the microSD filesystem!
5- connect the DSO with the PC with USB cable
6- windows users should check up "my computer" for new removable drive appeared.
6.1-If the new drive have appeared but you see window 'hang up' and too sloooow - this microSD card is inappropriate for your DSO. Return it to shop, get another one and repeat from step 1.
6.2-If windows says 'disk is unformatted - format now?' - its OK! Click YES, then select type FAT and do full (not quick) format of the flash card.
6.3- maybe you even see an empty disk - so you even dont have to format it.
7 - So you have seen a new drive and can access it from your PC. Pick up the archive DSO.zip attached below and extract files from it to the root folder of your microSD. Take a close attention: their names must contain small letters ONLY (i.e. config.dat not CONFIG.DAT). If not - simply rename it.
8. After all just cycle the power.If you see the mV values instead of Freq and Hz in the quick measure tab and the horizontal cursors are 0V and 5V - you are having success!
Attachments
DSO.zip
(1.01 KiB) Downloaded 342 times

Paul2
Pre-kindergarten
Pre-kindergarten
Posts: 14
Joined: Sat May 29, 2010 10:35 am

Re: Firmware 1.5

Post by Paul2 » Wed Sep 29, 2010 4:01 pm

Special for those who have no usable SD,but ref wave is limmited to 4,
also worked for those who have an usable SD.
Attachments
1.6.rar
(33.31 KiB) Downloaded 467 times

Post Reply