I have used the CBB-Serial cape with BBB to get CAN communication going on the BBB. Now I tried to use the same thing on BBG (Beaglebone Green), thinking the same pins are available. Somehow it does not work.
The CBB-Serial uses pin 24 (DCAN1_RX) and 26 (DCAN1_TX) on the P9 header, which should be available for BBG. I am puzzled by why it's not working.
Begalebone Green with CBB-Serial
Moderators: lily.li, violet, salmanfarisvp, seth.welday
-
- Staff
- Posts: 168
- Joined: Tue Jan 25, 2011 11:16 am
- Are you a staff member of seeedstudio?: no
- Which products/projects are your favorite?: Seeeduino Film,Motion Frame,UartSbee
Re: Begalebone Green with CBB-Serial
Hello,
We have never used CBB-Serial Cape before. Coud you please check if the way 5V_VDD works in BBG be the reason In CBB-Serial Cape scehmatic 5V is powered by 5V_VDD (which is not available in BBG due to lack of DC Jack port)
BBG pins works like BBB. Refer BBB System Reference Manual :
"VDD_5V is the main power supply from the DC input jack. This voltage is not present when the board is powered via USB. The amount of current supplied by this rail is dependent upon the amount of current available . Based on the board design, this rail is limited to 1A per pin from the main board.
SYS_5V rail is the main rail for the regulators on the main board. When powered from a DC supply or USB, this rail will be 5V. The available current from this rail depends on the current available from the USB and DC external supplies"
There is no DC input jack in BBG. Hence, VDD_5V is not present. Please refer BBG schematic for more details. There is a way to connect SYS_5V to VDD_5V by using a 0 Ohm resistor.
Thanks and Warm Regards.
We have never used CBB-Serial Cape before. Coud you please check if the way 5V_VDD works in BBG be the reason In CBB-Serial Cape scehmatic 5V is powered by 5V_VDD (which is not available in BBG due to lack of DC Jack port)
BBG pins works like BBB. Refer BBB System Reference Manual :
"VDD_5V is the main power supply from the DC input jack. This voltage is not present when the board is powered via USB. The amount of current supplied by this rail is dependent upon the amount of current available . Based on the board design, this rail is limited to 1A per pin from the main board.
SYS_5V rail is the main rail for the regulators on the main board. When powered from a DC supply or USB, this rail will be 5V. The available current from this rail depends on the current available from the USB and DC external supplies"
There is no DC input jack in BBG. Hence, VDD_5V is not present. Please refer BBG schematic for more details. There is a way to connect SYS_5V to VDD_5V by using a 0 Ohm resistor.
Thanks and Warm Regards.
Re: Begalebone Green with CBB-Serial
Hi,
Thanks for your quick response.
Yes, CBB-Serial does use the VDD_5V to power up the CAN transceiver.
Per your comments, we shorted out USB_DC and VDD_5V. We now have the CBB-Serial working.
Thanks again for your help.
Warm Regards.
Thanks for your quick response.
Yes, CBB-Serial does use the VDD_5V to power up the CAN transceiver.
Per your comments, we shorted out USB_DC and VDD_5V. We now have the CBB-Serial working.
Thanks again for your help.
Warm Regards.