ReSpeaker USB 4 Mic Array Questions

info about ReSpeaker series products

Moderators: lily.li, violet, seth.welday

Post Reply
aragorn7189
Pre-kindergarten
Pre-kindergarten
Posts: 1
Joined: Mon Jun 17, 2019 10:54 pm

ReSpeaker USB 4 Mic Array Questions

Post by aragorn7189 » Tue Jun 18, 2019 11:15 pm

Hello, I'm looking for help with a few questions I have for the USB 4 Mic Array.

1. Can your 2-dimensional array of 4 microphones (i.e., USB 4 Mic Array) be used to provide both azimuth and elevation angles for a sound source using software like ManyEars or ODAS

2. Assuming the sound source is loud enough and noise levels are low enough, is there any limit to the distance between sound source and mic array, beyond which your hardware won’t be able to give direction-of-arrival information?

I would greatly appreciate any help with these questions. Have a nice day!

bill.yu
Junior-6
Junior-6
Posts: 638
Joined: Mon Apr 02, 2018 11:05 am

Re: ReSpeaker USB 4 Mic Array Questions

Post by bill.yu » Wed Jun 19, 2019 3:12 pm

Hi there~

1. Can your 2-dimensional array of 4 microphones (i.e., USB 4 Mic Array) be used to provide both azimuth and elevation angles for a sound source using software like ManyEars or ODAS

The respeaker mic array v2.0 can work with ODAS. You can refer to wiki page.
http://wiki.seeedstudio.com/ReSpeaker_M ... d-tracking

2. Assuming the sound source is loud enough and noise levels are low enough, is there any limit to the distance between sound source and mic array, beyond which your hardware won’t be able to give direction-of-arrival information?

I just tested it around 10 meters and the DOA works well. thanks.

Post Reply